SLUU182A January 2004 – March 2022 TPS5124
The current limit in the TPS5124 is set using an internal current source and an external resistor (R13 and R14). The current limit protection circuit compares the drain-to-source voltage of the high-side and low-side drivers with respect to the set-point voltage. If the voltage exceeds the limit during high-side conduction, the current limit circuit terminates the high-side driver pulse. If the set point voltage is exceeded during low-side conduction, the low-side pulse is extended through the next cycle. Together, this action has the effect of decreasing the output voltage until the undervoltage protection circuit is activated and the fault latch is set and both the high-side and low-side MOSFET drivers are shut off. Equation 16 should be used for calculating the external resistor value for current protection set point.
where