SLUUC57B october 2019 – august 2023 BQ79600-Q1
The EVMs are connected using 4-position Molex connectors. The BQ79600EVM has a high side (J15)and low side (J14) communication connector available on each board. By default the isolation filters for the vertical interface on the BQ79600EVM are set to transformer isolation. There are also footprints on the board to populate a different transformer model. More details can be found in the schematic near the end of this user guide. To connect the BQ79600EVM to the BQ79616EVM using NORTH direction for communication, connect J15 on the BQ79600EVM to J10 on the BQ79616EVM. If several BQ79616EVMs are stacked, connect them as indicated in the EVM user's guide for the device. If using ring architecture, connect J11 of the top most BQ79616EVM to J14 on the BQ79600EVM.
| Connection Name | BQ79600EVM High Side | BQ79616EVM Low Side |
|---|---|---|
| COMH_N to COML_N | J15 pin 4 | J10 pin 1 |
| COMH_P to COML_P | J15 pin 3 | J10 pin 2 |
| Connection Name | BQ79600EVM Low Side | BQ79616EVM High Side |
|---|---|---|
| COML_N to COMH_N | J14 pin 1 | J11 pin 4 |
| COML_P to COMH_P | J14 pin 2 | J11 pin 3 |