SLUUC68A August 2020 – April 2021 TPS563207
The TPS563207EVM response to load transient is shown in Figure 4-9. The current steps are indicated in the figures. The loading step slew rate is 2.5 A/μs. Total peak-to-peak voltage variation is as shown.
Figure 4-9 Load Transient
Response, 10% to 90% Load Step