SLUUCY5A November 2023 – May 2025 BQ25756E
Navigate to the TI-CHARGER-GUI tool folder. Once at the tool page, click on the Evaluate in the cloud button. The browser automatically redirects to the TI Charger GUI landing page. From the landing page, locate the device desired for evaluation and click Select Device. Note that the EVM must be powered and the USB2ANY must be connected to both the EVM and the PC for a connection to be established. Also, update the USB2ANY to the latest version with the USB2ANY Explorer Software.