SLUUCY8 December 2023 BQ77307
If the BQ77307 device is used in a system with fewer than 7 series cells, specific cells must be used for connection to real cells, as shown in Table 6-2. Short out the unused cell inputs on the circuit board. The device only evaluates protections associated with those cells designated as real cells.
| Number of Cell Used (Vcell Mode setting) | Cell Connections | Shorted Cells |
|---|---|---|
| 0, 1, or 7 | VC7‒VC6, VC6‒VC5, VC5‒VC4, VC4‒VC3, VC3‒VC2, VC2‒VC1, VC1‒VC0 | none |
| 6 | VC7‒VC6, VC6‒VC5, VC5‒VC4, VC3‒VC2, VC2‒VC1, VC1‒VC0 | VC4‒VC3 |
| 5 | VC7‒VC6, VC5‒VC4, VC3‒VC2, VC2‒VC1, VC1‒VC0 | VC6‒VC5, VC4‒VC3 |
| 4 | VC7‒VC6, VC5‒VC4, VC3‒VC2, VC1‒VC0 | VC6‒VC5, VC4‒VC3, VC2‒VC1 |
| 3 | VC7‒VC6, VC5‒VC4, VC1‒VC0 | VC6‒VC5, VC4‒VC3, VC3‒VC2, VC2‒VC1 |
| 2 | VC7‒VC6, VC1‒VC0 | VC6‒VC5, VC5‒VC4, VC4‒VC3, VC3‒VC2, VC2‒VC1 |
Short the unused cell input pins to adjacent cell input pins, as shown in Figure 6-1.
It is also important to note that the range of voltages supported by the different VC pins differs depending on the pin. For example, pins VC7, VC6, and VC5 can only support cell protections if their pin voltage is greater than or equal to 2 V. Thus if implementing a 2s system using the top and bottom cell input pins, the upper cell voltage protections are not evaluated correctly if the bottom cell voltage drops below 2 V, because VC6 is below 2 V.
The Settings:Configuration:Vcell Mode data memory setting is used to specify which cell inputs are used for actual cells. The device uses this information to disable cell voltage protections associated with inputs which are not used.