SLVAE51A November 2018 – October 2020 LM7310 , TPS2100 , TPS2101 , TPS2102 , TPS2103 , TPS2104 , TPS2105 , TPS2110 , TPS2111 , TPS2111A , TPS2112 , TPS2112A , TPS2113 , TPS2113A , TPS2114 , TPS2114A , TPS2115 , TPS2115A , TPS2120 , TPS2121 , TPS25947
When switching between one supply to another, there are two possible outcomes:
If using a break-before-make power MUX, then switchover time is one key factor which will determine whether a seamless switchover will or will not occur. Faster switchover time will help achieve seamless switchover, at the expense of higher inrush current. This balance should be considered and power MUX solutions are available with a range of switchover times.
If using a diode-mode or make-before-break power MUX, then seamless switchover is often possible since worst-case output voltage drop will be approximately 0.4 V to 0.7 V (depending on the diode used).