SLVAF01 October 2020 TPS55340
If there is a strict requirement regarding to switching node waveform in the flyback converter, the user needs to check whether the reflected voltage is optimized at first and then consider proper snubbing methods. There also should not be a pcb design error that usually generates parasitic inductance in the critical path. Lastly, keeping correct measurements is also important to receive exact voltage waveform on SW node as well.