SLVAFU9 January   2025 TPS62840 , TPS62843

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Inverting Buck-Boost Topology
    1. 1.1 Concept
    2. 1.2 Output Current Calculations
    3. 1.3 VIN and VOUT Range
  5. 2Design Considerations
    1. 2.1 Additional Input Capacitor
    2. 2.2 Digital Input Pin Configurations
    3. 2.3 Startup Behavior and Switching Node Consideration
  6. 3External Component Selection
    1. 3.1 Inductor Selection
    2. 3.2 Capacitor Selection
  7. 4Typical Performance
  8. 5Summary
  9. 6References

Output Current Calculations

The average inductor current is also affected in this topology. In the buck configuration, the average inductor current is equal to the average output current because the inductor always supplies current to the load during both the on and off times of the control MOSFET. However, in the inverting buck-boost configuration, the load is supplied with current only from the output capacitor and is completely disconnected from the inductor during the on time of the control MOSFET. During the off time, the inductor connects to both the output capacitor and the load (see Figure 1-5). Knowing that the off time is (1 – D) of the switching period, Equation 1 can be used to calculate the average inductor current:

Equation 1. IL(Avg)=IOUT(1-D)

The operating duty cycle for an inverting buck-boost converter can be found with Equation 2:

Equation 2. D=VOUT(VOUT-VIN)×η

Rather than VOUT/VIN for a buck converter. The efficiency term in Equation 2 adjusts the equations in this section for power conversion losses and yields a more accurate maximum output current result. The peak-to-peak inductor ripple current is given by Equation 3:

Equation 3. ΔIL=VIN×DfS×L

where:

  • ΔIL (A): the peak-to-peak inductor ripple current
  • D: duty cycle
  • η: efficiency
  • fS (MHz): switching frequency
  • L (μH): inductor value
  • VIN (V): the input voltage with respect to ground, not with respect to the device ground or VOUT

Equation 4 calculates the maximum inductor current:

Equation 4. IL=IL(avg)+ΔIL2

For example, for an output voltage of –1.8V, 2.2μH inductor, and input voltage of 3.3V, the following calculations produce the maximum allowable output current that can be achieved based on the TPS62840 minimum current limit value of 1A. The efficiency term is estimated at 80 %.

Equation 5. D=VOUT(VOUT-VIN)×η=-1.8 V(-1.8 V-3.3 V)×0.8=0.441
Equation 6. ΔIL=VIN×DfS×L=3.3 V×0.4411.8 MHz×2.2 μH=368 mA

Rearranging Equation 4 and setting IL(max) equal to the minimum value of ILIMF, as specified in the data sheet, gives:

Equation 7. IL(avg)=IL(max)-ΔIL2=1000 mA-368 mA2=816 mA

This result is then used in Equation 1 to calculate the maximum achievable output current:

Equation 8. IOUT=IL(avg)×(1-D)=816 mA×(1-0.441)=456 mA

Table 1-1 provides several examples of the calculated maximum output currents for different output voltages (–1.8V, –1.5V and –1.2V) based on an inductor value and switching frequency of 2.2μH and 1.8MHz, respectively. Increasing the inductance and/or input voltage allows higher output currents in the inverting buck-boost configuration. The maximum output currents for the TPS62840 in the inverting buck-boost topology are frequently lower than 750mA due to the fact that the average inductor current is higher than that of a typical buck. The output current for the same three output voltages and different input voltages is displayed in Figure 1-6.

Table 1-1 Maximum Output Current Calculation for Different Values of VOUT
ParameterVOUT = -1.8VVOUT = -1.5VVOUT = -1.2V
VIN (V)3.33.33.3
η0.80.80.8
fs (MHz)1.81.81.8
L (μH)2.22.22.2
IL(max) (mA)100010001000
D0.4410.3910.333
ΔIL (mA)368326278
IL(avg) (mA)816837861
IOUT (mA)456510574
 Maximum Output Current versus VINFigure 1-6 Maximum Output Current versus VIN