SLVAFU9 January 2025 TPS62840 , TPS62843
The TPS62840 buck dc-to-dc converter can be configured as an inverting buck-boost converter to generate a negative output voltage. The inverting buck-boost topology changes some system characteristics, such as input voltage range and maximum output current. This application report explains the inverting buck-boost topology and how to select the proper values of external components with the changed system characteristics. TPS62840 also gives design guidelines and precautions to make sure the robust operation of the converter. Measured data from the example design are provided. This application report also applies to any of the devices in the TPS6284x family.