SLVSAX9G September 2011 – November 2025 DRV8818
PRODUCTION DATA
The DRV8818 supports three different decay modes: slow decay, fast decay, and mixed decay. The current through the motor windings is regulated using a fixed off time scheme.
This means that the current increases until reaching the current chopping threshold (ITRIP), after which the current enters the set decay mode for a fixed period of time. The cycle then repeats after the decay period expires.
The blanking time tBLANK defines the minimum drive time for the current chopping. ITRIP is ignored during tBLANK, so the winding current can overshoot the trip level.