SLVSFC9B October 2020 – March 2022 TPS25947
PRODUCTION DATA
The TPS25947xx implements Undervoltage Protection on IN in case the applied voltage becomes too low for the system or device to properly operate. The Undervoltage Protection has a default lockout threshold of VUVP which is fixed internally. Also, the UVLO comparator on the EN/UVLO pin allows the Undervoltage Protection threshold to be externally adjusted to a user defined value. The Figure 8-4 and Equation 1 show how a resistor divider can be used to set the UVLO set point for a given voltage supply.
Figure 8-4 Adjustable Undervoltage
Protection