SLVSFW1A December 2025 – October 2026 TPS1HC120-Q1
PRODMIX
The TPS1HC120-Q1 provides output short-circuit protection to establish that the device prevents current flow in the event of a low impedance path to GND, removing the risk of damage or significant supply droop. The device is established to protect against short-circuit events up to 28V supply.
Figure 7-4 shows the behavior of the TPS1HC120-Q1 when the device is enabled into a short circuit.
Once the device is enabled, due to the low impedance path, the output current rapidly increases until it hits the current limit threshold (ICL). Due to the response time of the current limiting circuit, the measured maximum current can temporarily exceed the ICL value defined as ICL_ENPS, however, it settles to the current limit regulation value. In this state, high power is dissipated in the FET, so eventually the internal thermal protection temperature for the FET is reached and the device safely shuts down. After thermal shut down:
Figure 7-5 shows the behavior of the TPS1HC120-Q1 when a short-circuit occurs while the device is in the on-state and already delivering current. When the internal pass FET is fully enabled, the current limiting response time is slower. So to validate that the current overshoot is limited, the device implements a fast trip at a level IOVCR. When this fast trip threshold is hit, the device immediately shuts off for a short period of time before quickly re-enabling and clamping the current to ICL level after a brief transient overshoot to the higher peak current (ICL_ENPS) level. The device then keeps the current clamped at the regulation current limit until the thermal shutdown temperature is hit and the device safely shuts off. Once thermal shutdown is hit, the device latches off until the enable inputs toggle if the output voltage is less than 3V, and retries if the output voltage is more than 3V.
Once the device re-enables due to enable input toggling, if the output short still exists, the scenario is identical to the enable into permanent short scenario.
Figure 7-6 shows the behavior of the TPS1HC120-Q1 when there is a small change in impedance that sends the load current above the ICL threshold. The current rises to ICL_LINPK above the regulation level. Then the current limit regulation loop kicks in and the current drops to the ICL value.
In all of these cases, the internal thermal shutdown is safe to hit repetitively. There is no device risk or lifetime reliability concerns from repeatedly hitting this thermal shutdown level.