SLVSH61C March 2025 – November 2025 TPS7H4102-SEP , TPS7H4104-SEP
PRODMIX
To calculate the value of the output inductor, use Equation 28. KLx is a coefficient that represents the amount of inductor ripple current relative to the maximum output current, IOUTx as shown in Equation 29. Since the output capacitors must have a ripple current rating greater than or equal to the inductor ripple current, choosing a high inductor ripple current impacts output capacitors selection. In general, the inductor ripple value is at the discretion of the designer depending on specific system needs. Typical values for KLx range from 10% to 50%. For low output currents, the value of KL x can be increased to minimize excessive switch (SWx) jitter and to reduce the value of the output inductor.
For this design example, use KLx = 40% and VIN_MAX = 5.5V (5V + 10%). Once the inductor value is known (or selected) the actual ripple current (ΔiLx), RMS and peak current can be calculated, using Equation 30, Equation 31 and Equation 32, respectively. The inductor design details are presented in Table 9-2.
| VOUTx (V) | CALCULATED INDUCTOR VALUE (μH) | SELECTED INDUCTOR VALUE (μH) | INDUCTOR RIPPLE CURRENT (A) | INDUCTOR RMS CURRENT (A) | INDUCTOR PEAK CURRENT (A) |
|---|---|---|---|---|---|
| 0.8 | 1.14 | 1.8 | 0.76 | 3.01 | 3.38 |
| 1.2 | 1.56 | 1.8 | 1.04 | 3.02 | 3.52 |
| 1.5 | 1.82 | 1.8 | 1.21 | 3.02 | 3.61 |
| 1.8 | 2.02 | 2.2 | 1.10 | 3.02 | 3.55 |
The current flowing through the inductor is the inductor ripple current plus the output current. During power up, faults, or transient load conditions, the inductor current can increase above the previously calculated peak inductor current level. In transient conditions, the inductor current can increase up to the switch current limit of the device. For this reason, the most conservative approach is to specify an inductor with a saturation current rating equal to or greater than the maximum switch current limit, rather than the peak inductor current.
For the TPS7H410x the maximum value for the current limit is dominated by the IOC_LS_SOURCINGx at 7.6A. The selected inductor model, saturation current, and the RMS are shown in Table 9-2.
| INDUCTOR VALUE (μH) | INDUCTOR PART NUMBER | INDUCTOR ISAT RATING (A) | INDUCTOR IRMS RATING (A) |
|---|---|---|---|
| 1.8 | XGL6030-182MEC | 9.4 | 9.5 |
| 2.2 | XGL6030-222MEC | 8.7 | 8.5 |