SLVSHO8 May 2026 TPS26741E-Q1
PRODUCTION DATA
The TPS26741E-Q1 supports being connected to multiple other PD controllers to enable system power sharing across multiple ports. One of the TPS26741E-Q1 is configured as the Controller, and the other is configured as a Target. In the following diagram the I2C2 port from one device is connected to the I2C3 port from another device. Since the I2C2 is the controller port, it makes that device the Controller in the SPM context as well.
The SPM controller also handles power sharing for all ports within the SPM controller.