SLVSHR6A July 2025 – November 2025 TPS1686
PRODUCTION DATA
The TPS1686x implements Undervoltage Lockout on VDD and VIN in case the applied voltage becomes too low for the system or device to properly operate. The Undervoltage lockout has a default lockout threshold of VUVP internally on VDD and VUVPIN on VIN. Also, the UVLO comparator on the EN/UVLO pin allows the Undervoltage Protection threshold to be externally adjusted to a user defined value. The following figure and equation show how a resistor divider can be used to set the UVLO set point for a given voltage supply.
Figure 7-1 Adjustable Undervoltage ProtectionThe EN/UVLO pin implements a bi-level threshold.