SLVSHR6A July 2025 – November 2025 TPS1686
PRODUCTION DATA
Selecting the CDVDT capacitor to control the output slew rate and start-up time
A capacitor (CDVDT) must be added at the DVDT pin to GND to set the required value of slew rate. Equation 10 is used to compute the value of CDVDT.
To get slew rate of 1V/ms , as per above equation we get CDVDT as 50nF. Keep the nearby standard value of 47nF.
Selecting the RIREF resistor to set the reference voltage for overcurrent protection.
. Equation 11 is used to calculate the value of RIREF.
In this design example, VIREF is set at 1V. With IIREF = 25µA (typical), calculate the target RIREF to be 40kΩ. The closest standard value of RIREF is 40.2kΩ with 0.1% tolerance and power rating of 100mW. For improved noise immunity, place a 100pF ceramic capacitor from the IREF pin to GND.
Maintain VIREF within the recommended voltage to verify the proper operation of overcurrent detection circuit.
Selecting the RIMON resistor to set the overcurrent (circuit-breaker) and fast-trip thresholds during steady-state
TPS1686x eFuse responds to the output overcurrent conditions during steady-state by turning off the output after a user-adjustable transient fault blanking interval. This eFuse continuously senses the total system current (IOUT) and produces a proportional analog current output (IIMON) on the IMON pin. This generates a voltage (VIMON) across the IMON pin resistor (RIMON) in response to the load current, which is defined as Equation 12.
GIMON is the current monitor gain (IIMON : IOUT), whose typical value is 18.2µA/A. The overcurrent condition is detected by comparing the VIMON against the VIREF as a threshold. The circuit-breaker threshold during steady-state (IOCP) can be calculated using Equation 13.
In this design example, IOCP is considered as 10A, and RIMON can be calculated to be 5.5kΩ with GIMON as 18.2µA/A and VIREF as 1V. The nearest value of RIMON is 5.6kΩ with 0.1% tolerance and power rating of 100mW. For noise reduction, place a 22pF ceramic capacitor across the IMON pin and GND.
Selecting the CITIMER capacitor to set the overcurrent blanking timer
An appropriate capacitor must be connected at the ITIMER pin to ground of the primary or standalone device to adjust the duration for which the load transients above the circuit-breaker threshold are allowed. The transient overcurrent blanking interval can be calculated using Equation 14.
Where tITIMER is the transient overcurrent blanking timer and CITIMER is the capacitor connected between ITIMER pin of the device and GND. IITIMER = 2µA (typical) and ΔVITIMER = 1.55V (typical). A 4.7nF capacitor with 10% tolerance and DC voltage rating of 25V is used as the CITIMER for the device in this design.
Selecting the resistors to set the undervoltage lockout threshold
The undervoltage lockout (UVLO) threshold is adjusted by employing the external voltage divider network of R1 and R2 connected between IN, EN/UVLO, and GND pins of the device as described in undervoltage protection section. The resistor values required for setting up the UVLO threshold are calculated using Equation 15.
To minimize the input current drawn from the power supply, TI recommends using higher resistance values for R1 and R2. From the device electrical specifications, UVLO rising threshold VUVLO(R) = 1.2V. From the design requirements, VINUVLO = 46V. First choose the value of R1 = 3.74MΩ and use Equation 15 to calculate R2 = 100kΩ. Use the closest standard 1 % resistor values: R1 = 3.74MΩ and R2 = 100kΩ. For noise reduction, place a 100pF ceramic capacitor across the EN/UVLO pin and GND.
Selecting the resistors to set the overvoltage lockout threshold
The overvoltage lockout (OVLO) threshold is adjusted by employing the external voltage divider network of R3 and R4 connected between IN, OVLO, and GND pins of the device as described in the overvoltage protection section. The resistor values required for setting up the OVLO threshold are calculated using below equation.
To minimize the input current drawn from the power supply, TI recommends using higher resistance values for R3 and R4. From the device electrical specifications, OVLO rising threshold VOVLO(R) = 1.17V. From the design requirements, VINOVLO = 60V. First choose the value of R1 = 5.11MΩ and use Equation 15 to calculate R3 = 101kΩ. Use the closest standard 1% resistor values: R3 = 5.11MΩ and R4 = 102kΩ. For noise reduction, place a 10pF ceramic capacitor across the OVLO pin and GND.
Selecting the R-C filter between VIN and VDD
VDD pin is intended to power the internal control circuitry of the eFuse with a filtered and stable supply, not affected by system transients. Therefore, use an R (150Ω) – C (0.22µF) filter from the input supply (IN pin) to the VDD pin. This helps to filter out the supply noises and to hold up the controller supply during severe faults such as short-circuit at the output. In a parallel chain, this R-C filter must be employed for each device.
Selecting the pullup resistors and power supplies for FLT,
FLT is the open drain output. If these logic signal is used, the signal must be pulled up to an appropriate supply rail voltage through 33kΩ pullup resistances.
Selection of TVS diode at input and Schottky diode at output
In the case of a short circuit and overload current limit when the device interrupts a large amount of current instantaneously, the input inductance generates a positive voltage spike on the input, whereas the output inductance creates a negative voltage spike on the output. The peak amplitudes of these voltage spikes (transients) are dependent on the value of inductance in series with the input or output of the device. Such transients can exceed the absolute maximum ratings of the device and eventually lead to failures due to electrical overstress (EOS) if appropriate steps are not taken to address this issue. Typical methods for addressing this issue include:
Refer to TVS Clamping in Hot-Swap Circuits , Selecting TVS Diodes in Hot-Swap and ORing Applications, TVS Diode recommendation tool for details on selecting an appropriate TVS diode and the number of TVS diodes to be in parallel to effectively clamp the positive transients at the input below the absolute maximum ratings of the IN pin (90V). These TVS diodes also help to limit the transient voltage at the IN pin during the Hot Plug event. One(1) SMDJ54A is used in this design example.
Maximum Clamping Voltage VC specification of the selected TVS diode at Ipp (10/1000μs) (V) must be lower than the absolute maximum rating of the power input (IN) pin for safe operation of the eFuse.
Selection of the Schottky diodes must be based on the following criteria:
1 B360-13-F is used in this design example.
TI recommends to add ceramic bypass capacitors to help stabilize the voltages on the input and output. The value of CIN must be kept small to minimize the current spike during hot-plug events. For each device, 0.01µF of CIN is a reasonable target. Because COUT does not get charged during hot-plug, a larger value such as 10µF can be used at the OUT pin of each device.