SLVSI54 May 2025 TPS60800-Q1
PRODUCTION DATA
As given in Thermal Information, the thermal resistance RΘJB of TPS60800-Q1 is 109.1°C/W. RΘJB refers to the thermal resistance between the device junction temperature and the surrounding board temperature. The following equations calculate the highest allowable board temperature under full power conditions, subject to the device junction temperature not exceeding 125°C.
The thermal resistance RΘJB can be calculated using Equation 7.
where:
TJ is the junction temperature, TB is the board temperature and PD is the power dissipated by the device.
The maximum power dissipation can be calculated by using the following Equation 8.
The maximum power dissipation happens with maximum input voltage and maximum output current.
At maximum load the maximum supply current is 1mA (see Equation 9).
With this maximum power rating and thermal resistance, RΘJB, the maximum junction temperature rise above the board temperature can be calculated using Equation 10.
This equation means that the power dissipation increases TJ by < 20°C with respect to the board temperature.
The junction temperature of the device must not exceed 125°C.
This limit implies the IC can easily be used up to board temperatures given by Equation 11.