SLVSIC8 December 2025 TPSM852892
PRODUCTION DATA
In boost mode, the output capacitor conducts high ripple current. The output capacitor RMS ripple current is given by Equation 15, where the minimum input voltage and the maximum output voltage correspond to the maximum capacitor current.

where
In this example, the maximum output ripple RMS current is 1.7A.
The ESR of the output capacitor causes an output voltage ripple given by Equation 16 in boost mode.

where
The capacitance also causes a capacitive output voltage ripple given by Equation 17 in boost mode. When input voltage reaches the minimum value and the output voltage reaches the maximum value, there is the largest output voltage ripple caused by the capacitance.

Typically, a combination of ceramic capacitors and bulk electrolytic capacitors is needed to provide low ESR, high ripple current, and small output voltage ripple. From the required output voltage ripple, use Equation 16 and Equation 17 to calculate the minimum required effective capacitance of the COUT.
Add a 0.1μF/0402 package ceramic capacitor and place it close to VOUT pin and GND pin to suppress high frequency noise which helps improve EMI performance.