The operational area of an LDO is limited by the
dropout voltage, output current, junction temperature, and input voltage. The recommended
area for continuous operation for a linear regulator is provided in Figure 7-3 and can be separated into
the following regions:
- Dropout voltage limits the minimum differential
voltage between the input and the output (VIN – VOUT) at a given
output current level; see the Dropout Operation section for more details.
- The rated output current limits the maximum recommended output current level. Exceeding this rating causes the device to fall out of specification.
- The rated junction temperature limits the maximum junction temperature of the device. Exceeding this rating causes the device to fall out of specification and reduces long-term reliability.
- Equation 6 provides the shape of the slope. The slope is nonlinear because the maximum rated junction temperature of the LDO is controlled by the power dissipation across the LDO, thus when VIN – VOUT increases the output current must decrease.
- The rated input voltage range governs both the minimum and maximum of VIN – VOUT.