SLVSL58 September 2026
ADVANCE INFORMATION
Figure 2-4 shows the Texas Instruments TXB0104, a 4-bit bidirectional voltage-level shifter with auto direction sensing. The EVM uses the TXB0104 to translate voltage levels between the controller and the ADC. This translation decouples the ADC supply voltage from the controller I/O voltage so the user can power the EVM to enable higher input voltage measurements. For example, the user can set the ADC_VDD to 5V to measure larger signals while keeping the communication voltage (IO_VDD) at 3.3V