SLVT229 December 2025
The following hardware is required for this reference design:
The following test equipment is needed to power and evaluate the DUT:
Thermal interface material (TIM) needs to be applied in between the aluminum heatsink and the exposed copper plane to maintain proper contact between surfaces and also avoid direct short across different power nets.
Figure 3-1 Dimension of the
Heatsink
Figure 3-2 Bottom Side of
PMP41150