SLVT229 December 2025
Reverse step-up operation is observed (shown in Figure 3-17) via the measurement on the SW node voltage of bias buck converter. Vsw here is an indication of whether the 48V on the input (which at the same time is the HV port of the SCC) has been established or not).
Here before the cursor "b" timestamp, the peak of SW node voltage has always been following the 12V input from the LV port (which is the output port for step-down operation).
After the "b" timestamp, the peak of SW node has risen as the reverse step-up operation is charging the HV port capacitors and raising HV voltage. By the time of the cursor "a" timestamp, the reverse operation has been done.
Figure 3-17 Reverse Operation, 1:4 Conversion Ratio, VLV = 12V, SCC Load = 300W.