SLVUBT0A June 2020 – January 2021
As shown in Figure 3-4, multiple boards can be configured into a master-slave relationship (1 master and up to 5 slaves) and physically stacked upon each other. VCCA and GND are shared between boards on headers J27 and J28. Communication between the boards is shared on header J29. This header, J29, is marked on the bottom silkscreen, as shown in Figure 3-5.
Figure 3-4 EVM
Masters Slave Configuration
Figure 3-5 EVM Bottom View Version 2The J29 signal, nPWRON_S, and the nPWRON/ENABLE or VOUT_LDOVINT signals of the PMIC are connected through J37. When multiple PMICs are stacked, as shown in Figure 3-6, the expectation is that the master is placed in master mode, connecting the stackable signal nPWRON_S, and the VOUT_LDOVINT. By using this stackup configuration, one or more of the slaves power up sequence will always follow the master. When in master mode or when the header J37 is left open the nPWRON/ENABLE pin can be controlled with the EVM push button, S1, or the jumper J45.(1)
Figure 3-6 Header J37 Master and Slave Select
Table Description for 'OPEN' configuration| Configuration | Description |
|---|---|
| Open | When used as a single PMIC (no stacking). ENABLE is connected to a pullup and therefore automatically enabled. S1 can be used to generate edges or J45 at any level.(1) |
| Slave, M/S Select: Closed | Slave Mode. The PMIC signal ENABLE is connected to the nPWRON_S signal which is from the master's VOUT_LDOVINT. |
| M/S Select, Master: Closed | Master Mode. The PMIC signal, VOUT_LDOVINT, is connected to the nPWRON_S which will be the ENABLE signal on the PMICs connected as slaves. |