SLVUBT0A June   2020  – January 2021

 

  1.   1
  2.   2
  3.   3
    1.     4
    2.     5
    3.     6
  4.   7
    1.     8
    2.     9
    3.     10
    4.     11
    5.     12
    6.     13
    7.     14
    8.     15
  5.   16
    1.     17
    2.     18
  6.   19
  7.   20
  8.   21

The GUI Tool

Texas Instruments provides a GUI tool to enable, configure, and evaluate the various features of the TPS6594x-Q1 with the EVM. Please refer to the GUI User's Guide SLVUBT8 for a more detailed description of this tool.

The GUI will run on most PC platforms and requires an available USB port. The EVM USB connector is type-C and a type-A to type-C cable is provided with the EVM to connect to the host computer. The EVM will enumerate as two COM ports and one additional port for the devices firmware updates. The port the GUI should use is the ACCtrl COM port (and not the ACCtrl Console).