SLVUBT1A October   2019  – June 2020 TPS50601A-SP

 

  1.   TPS50601A-SP Worst Case Analysis Unencrypted PSpice Average Model User's Guide
    1.     Trademarks
    2. 1 TPS50601A-SP WCA Model Specification
    3. 2 Default Parameters
    4. 3 Example of using model with Cadence Pspice (17.2.0)
      1. 3.1 Creating a part from the netlist file
      2. 3.2 Steps to create project in Capture
      3. 3.3 Creating the schematic in Capture
    5. 4 Simulating the Model
      1. 4.1 Monte Carlo Analysis of Output Voltage
      2. 4.2 Frequency Response Analysis
        1. 4.2.1 Analyzing Frequency Response with Bode Plot
        2. 4.2.2 Analyzing Frequency Response with Histogram
  2.   Revision History

TPS50601A-SP Worst Case Analysis Unencrypted PSpice Average Model User's Guide

This user's guide is intended to demonstrate use of the average Pspice model for the TPS50601A-SP synchronous buck converter. Instructions on importing the unencrypted model netlist into Cadence Pspice® are also provided. The first half of the guide outlines the modeled parameters and specifications and the second half of the guide addresses how to simulate the modeled parameters.