SLVUCT6 February 2024 TPS61299
The TPS61299 is a synchronous boost converter with 95nA ultra-low quiescent current and average input current limit. The device support both WCSP and SOT package; the latter is integrated in this EVM. The output current mainly depends on the input voltage, because the inductor peak current is limited at typical 1.2A. The EVM supports typical 0.8A from a 3.6V input voltage.
This user's guide describes the schematic, layout, bill of materials (BOM), and setup of the evaluation module (EVM) for the TPS61299.
![]() |
| Hot surface! Contact can cause burns. Do not touch! |