SLVUCZ6 November   2024 TLC69627-Q1 , TLC69628-Q1 , TLC69629-Q1 , TLC69637-Q1 , TLC69638-Q1 , TLC69639-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Software Setup
  6. 3Sample Code Structure
    1. 3.1 Design Parameters
    2. 3.2 Flow Diagram
    3. 3.3 Basic System Setup
    4. 3.4 Advanced System Setup
    5. 3.5 Diagnostics
    6. 3.6 Demo

Software Setup

To set up the software for the TMS320F280039C LaunchPad™, follow these steps (demonstrated in a computer with Windows 10 OS):

  1. Download and install Code Composer Studio™ (CCS).
    1. Download Code Composer Studio integrated development environment (IDE) (Version 12.7.0).
    2. Follow the installation instructions to install Code Composer Studio. During the installation process, if you choose the "Setup type" to be "Custom Installation", make sure that you select "C2000 real-time MCUs" in "Select Components", as is marked with red box in Figure 2-1.
       Installation Process of Code
                  Composer Studio Figure 2-1 Installation Process of Code Composer Studio
  2. Download and install C2000Ware (Version 5.02.00.00).
    1. To verify the installation is correct, open the Code Composer Studio software. Click "Windows" from the top menu bar. Then click "Preferences" from the drop-down list. The "Preferences" window will show. From the left side bar, select "Code Composer Studio" -> "Products".
    2. Make sure that there is "C2000Ware 5.2.0.00" and "SysConfig" (SysConfig should be installed automatically when you install C2000Ware) under the "Discovered products", as is marked in Figure 2-2. If there is no "C2000Ware 5.2.0.00" or "SysConfig" appearing, you may need to click "Refresh" on the right side of the "Preference" window. If still unavailable, check whether the installation is correct. A standalone desktop version of SysConfig can be found at SYSCONFIG System configuration tool.
       Verification of C2000Ware
                  5.02.0.00 Installation Figure 2-2 Verification of C2000Ware 5.02.0.00 Installation
  3. Download and import sample code.
    1. Importing the Code Composer Studio (CCS) project according to the process provided in the link: Importing a CCS Project.
  4. Before loading and running the program, switch S2 on LAUNCHXL-F280039C for both SEL1 and SEL2 should be set to the 1-position.
  5. Load the program according to the process provided in the link: Building and Running Your Project.