SLVUD02A April 2025 – May 2026
For the following tests, J32 is left open to ground the MODE pin to select 2x Undervoltage + 2x Overvoltage monitoring mode. Voltages are kept in regulation for the pair of channels not shown in the scope capture. Different DLY_TMR settings are shown.
Figure 3-4 Channel 1/2 Regulation
Monitoring with DLY_TMR floating
Figure 3-5 Channel 3/4 Regulation
Monitoring with DLY_TMR floating
Figure 3-6 Channel 3/4 Enter Regulation
with DLY_TMR=619kOhms
Figure 3-7 Channel 3/4 Leave Regulation
with DLY_TMR=619kOhms