SLVUD02A April 2025 – May 2026
The TPS7H3xx4EVM-CVAL boards are by default configured for the specific IC they feature. These configurations are minor BOM differences, which are listed below and also highlighted in the EVM schematic. Users can re-configure the boards for testing the other IC variants if desired. The board layouts are the same.
Pin configuration
TPS7H30x4-SP (push-pull variants) use 0-ohm resistors to connect the PULL_UPx pins (pin 17 and pin 18) to the PULL_UPx rails
TPS7H31x4-SP (open-drain variants) use 0-ohm resistors to connect pin 17 and pin 18 to GND and VLDO as required by the datasheet
External pull-up resistors
TPS7H30x4-SP (push-pull variants) depopulate the 6 external pull-up resistors used for the RESETxb, PWRGD, and WDOb outputs
TPS7H31x4-SP (open-drain variants) populate 6 external pull-up resistors used for the RESETxb, PWRGD, and WDOb outputs. The board uses 10k resistors as a default.