SLVUD79 July   2025

 

  1.   1
  2.   Description
  3.   Features
  4.   Applications
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Setup
  8. 3Hardware Design Files
    1. 3.1 Schematic
    2. 3.2 PCB Layout
    3. 3.3 Bill of Materials
  9. 4Additional Information
    1.     Trademarks

Schematic

Figure 3-1 shows the schematic of the TPSM81299EVM-119. Use a jumper cap on J5 to connect different resistors for different output voltages (refer to Figure 3-2 for more details). The tantalum capacitor, C3, is used to stabilize the input voltage for the TPSM81299, in case the cable between the power supply and the EVM is too long. In most applications, the tantalum capacitor is unnecessary. The definition of the connectors is explained as follows:

  • PIN 1 and PIN 2 of J1 are used for the ground of the input power supply.
  • PIN 5 and PIN 6 of J1 are used for the positive input of the power supply.
  • PIN 3 and PIN 4 of J1 are used to sense the input voltage closed to the IC (see the PCB; Section 3.2).
  • PIN 1 and PIN 2 of J4 are used for the negative input of the load.
  • PIN 5 and PIN 6 of J4 are used for the positive input of the load.
  • PIN 3 and PIN 4 of J4 are used to measure the output voltage closed to the IC (see the PCB; Section 3.2).
  • JP2 is used to enable or disable the IC through the EN pin.
  • JP3 is used to connect AVIN to the input rail or external aux input.
  • JP5 is used to select different output voltage with a jumper cap.
TPSM81299EVM TPSM81299EVM-119 Schematic Figure 3-1 TPSM81299EVM-119 Schematic