Downloading USB2ANY Firmware version
2.8.2.0 or higher is required for USB2ANY Explorer and TXE81XXEVM-GUI to work.
Note: The TXE81XXEVM is already flashed from the factory with
the latest firmware version (2.8.2.0). If the EVM is not connecting to the
USB2ANY Explorer, or is having connection issues with the full function GUI,
then follow these steps to reflash the device:
To check if the EVM has the updated
firmware, follow steps 1-4 below.
- Download USB2ANY Explorer Software (SLVC695) from ti.com.
- Run "USB2ANY Explorer-2.8.2.0
Setup" Application File and install the explorer GUI.
- Once the install is complete,
open USB2ANY Explorer.
- The USB2ANY Explorer GUI shows
the type, serial #, and firmware version underneath the "Adapter Connection" in
the GUI. The firmware version reads 2.8.2.0. If the "Firmware Version" shows
2.8.2.0, then the board is ready for use for either USB2ANY Explorer GUI or
TXE81XXEVM GUI use. If it does not, follow step 5.
- Disconnect the TXE81XXEVM from
the computer.
- Short
jumper J18 on the bottom side of the EVM. This sets up the USB2ANY
circuit into programming mode.
- Re-connect the EVM.
- Remove jumper on J18.
- Select "Open Device" in the
USB2ANY Explorer GUI and select "Yes".
- Select
"Update Firmware".
- Firmware
is flashed when the final message says "Done!"
- The Firmware Version underneath
"Adapter Connection" now reads 2.8.2.0. The USB2ANY circuit on the bottom side
of the EVM is now correctly flashed and ready for use in the USB2ANY Explorer
GUI or TXE81XXEVM GUI.