SLVUDG6 November 2025
The AWR2188EVM includes a 3D waveguide antenna by Huber+Suhner for the 16 receivers and 16 transmitters. This antenna design utilizes a near-regular array which enables estimation of both azimuth and elevation angles, allowing for object detection in a 3-D plane
Figure 2-13 Antenna Port AssignmentThe virtual array of the 16 transmitters is shown in the TX Virtual Array figure.
Figure 2-14 TX Virtual ArrayThe virtual array of the 16 receivers is shown in the RX Virtual Array figure.
Figure 2-15 RX Virtual Array
Figure 2-16 Antenna Near-Regular Array Configuration
Figure 2-17 TX and RX Simulated Directivity