SLVUDN3 December 2025
The TLV672XEVM contains resistors and switches at the INT/RSTn and LPWn/PRSn nodes to demonstrate in-application behavior. Input behavior is described below assuming V_HOST is powered by 3.3V.
The TLV672XEVM has test-points TP11 and TP18 at the INT/RSTn and LPWn/PRSn inputs of the TLV6722. These test points can be used to drive the INT/RSTn and LPWn/PRSn nodes directly if the user wants to bypass the input resistors and switches. If bypassing the input switches and resistors, the user still powers V_HOST and drive H_RSTn to 3.3V to avoid shorting the INT/RSTn driver to ground.
Another way to evaluate the TLV6722 is to configure the TLV672XEVM to have the device only. The user can depopulate R4, R9, and R7, as well as connecting V_HOST to GND to remove the effects of the host-side passives.
M_INT is the digital input to the TLV6722 that determines the connection of the internal 8kΩ resistor in the INT/RSTn circuit. M_INT behavior is described below.