SLVUDN5 January 2026
This procedure details how to configure the BQ25785 evaluation board. For the test procedure, the following naming conventions are followed. Refer to Section 3.1 for details.
| VXXX: | External voltage supply name (VIN, VSYS, VBAT). | |
| LOADy: | External load name (LOADy). | |
| V(TPyyy): | Voltage at internal test point TPyyy. For example, V(TP12) means the voltage at TP12. | |
| V(Jxx): | Voltage at jack terminal Jxx. | |
| V(TP(XXX)): | Voltage at test point “XXX”. For example, V(ACDET) means the voltage at the test point which is marked as “ACDET”. | |
| V(XXX, YYY): | Voltage across point XXX and YYY. | |
| I(JXX(YYY)): | Current going out from the YYY terminal of jack XX. | |
| Jxx(BBB): | Terminal or pin BBB of jack xx. | |
| JPxx ON : | Internal jumper JPxx terminals are shorted. | |
| JPxx OFF: | Internal jumper JPxx terminals are open. | |
| JPxx (-YY-) ON: | Internal jumper JPxx adjacent terminals marked as “YY” are shorted. | |
| Measure: → A,B | Check specified parameters A, B. If measured values are not within specified limits, the device under test has failed. | |
| Observe → A,B | Observe if A, B occurs. If A or B does not occur, the device under test has failed. |
Section 3.2 have locations for jumpers, test points, and individual components.