The multiplying THD is evaluated using
either of the following methods:
- External Precision Source: Use a
low-distortion sinusoidal source (for example, APx555) as the DAC reference input.
- Configure the DAC in multiplying mode
by clicking on the configure tab of the GUI.
- Apply the external signal to the
channel 1 reference SMA (J2).
- Measure the DAC output at channel 1
SMA (J4) using a distortion analyzer (APx555).
- AWG loopback of channel 0:
- Open the AWG page and generate the
desired sine wave.
- The GUI automatically configures
channel 0 in AWG mode and channel 1 in multiplying mode.
- Connect the channel 0 Output SMA (J3)
to the channel 1 reference SMA (J2) using a SMA to SMA cable.
- Measure the DAC output at channel 1
SMA (J4)) using a distortion analyzer (APx555).