SLVUE37 October   2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 System Description
      1. 1.3.1 Key System Specifications
      2. 1.3.2 End Equipment
      3. 1.3.3 Electricity Meter
      4. 1.3.4 Power Quality Meter, Power Quality Analyzer
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 System Overview
      1. 2.1.1 Block Diagram
      2. 2.1.2 Design Considerations
        1. 2.1.2.1 Voltage Measurement - Analog Front End
        2. 2.1.2.2 Current Measurement - Analog Front End
        3. 2.1.2.3 Input Voltage
        4. 2.1.2.4 XDS110 Emulator
        5. 2.1.2.5 Magnetic Tamper Detection With TMAG5273 Linear 3D Hall-Effect Sensor (Not Populated on EVM)
  9. 3Software
    1. 3.1 Metrology Overview
      1. 3.1.1 Metrology Formulas
      2. 3.1.2 UART for PC GUI Communication
      3. 3.1.3 Direct Memory Access (DMA)
      4. 3.1.4 ADC Setup
      5. 3.1.5 Foreground Process
      6. 3.1.6 Background Process
      7. 3.1.7 Software Function per_sample_dsp ()
      8. 3.1.8 Frequency Measurement and Cycle Tracking
      9. 3.1.9 LED Pulse Generation
  10. 4Implementation Results
    1. 4.1 Evaluation Procedure
      1. 4.1.1 Equipment Setup
        1. 4.1.1.1 Jumper Settings for LED and UART
        2. 4.1.1.2 Power Supply Options and Jumper Settings
      2. 4.1.2 Test Procedure
        1. 4.1.2.1 Working With the Metrology GUI
        2. 4.1.2.2 Calibration
          1. 4.1.2.2.1 Voltage and Current Offset Calibration
          2. 4.1.2.2.2 Voltage and Current Gain Calibration
          3. 4.1.2.2.3 Active Power Gain Calibration
          4. 4.1.2.2.4 Offset Calibration
          5. 4.1.2.2.5 Phase Calibration
    2. 4.2 Performance Data and Results
      1. 4.2.1 Electricity Meter Metrology Accuracy Results
      2. 4.2.2 Radiated Emissions Performance
        1. 4.2.2.1 EMI Mitigation Recommendations
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Additional Information
    1. 6.1 Trademarks
  13. 7Tools and Software
  14. 8Related Documentation
Phase Calibration

After performing power gain correction, do the phase calibration. To perform phase correction calibration, complete the following steps:

  1. If the AC test source has been turned OFF or reconfigured, perform steps 1 through 3 from Section 4.1.2.2.2 using the identical voltages and currents used in that section.
  2. Modify only the phase-shift to a non-zero value; typically, +60° is selected. The reference meter now displays a different % error for active power measurement.
    Note: This value can be negative.
  3. If the error from 2 is not close to zero, or is unacceptable, perform phase correction by following these steps:
    1. Enter a value as an update for the Phase correction field for the phase that is being calibrated. Typically, a small ± integer must be entered to bring the error closer to zero. Additionally, for a phase shift greater than 0 (for example: +60°), a positive (negative) error requires a positive (negative) number as correction.
    2. Click on the Update meter button and monitor the error values on the reference meter.
    3. If this measurement error (%) is not accurate enough, fine-tune by incrementing or decrementing by a value of 1 based on 1. After a certain point, the fine-tuning only results in the error oscillating on either side of zero. The value that has the smallest absolute error must be selected.
    4. Change the phase now to –60° and check if this error is still acceptable. In best practice, errors must be symmetric for the same phase shift on lag and lead conditions.

After performing phase calibration, calibration is complete. Figure 4-6 shows the new calibration factors.

AMC-ADC-3PH-EVM Calibration Factors WindowFigure 4-6 Calibration Factors Window