SLVUE37 October 2026
Figure 2-1 depicts the MSPM0G3507 and AMC131M03-based three-phase energy measurement application block diagram.
On each phase (or line) the line-to-neutral voltage is directly measured, as well as the current for each line (3 phases) and through the N (Neutral) wire; hence, both 3-phase, 3-wire (3P3W) or 3-phase, 4-wire with Neutral (3P4W) configurations are supported by default. By not using some phases, this reference design can also be used in a split-phase (leave open Phase C) or single-phase (leave open Phase B and C) configuration. In the TIDA-010244 block diagram, shunt sensors connect to each of the 3 phases for the current measurement while a simple voltage divider is used for dividing down the corresponding voltage of each line. The selection of the shunt is made based on the current range required for the energy measurements, while minimizing power dissipation in the shunt at high currents. Values in the range of 150μΩ to 200μΩ are common, assuming up to 100A or 120A maximum current per phase are to be measured.
In this design, the four AMC131M03 or AMC131M02 devices interact with the MSPM0+ MCU in the following manner:
The MSPM0+ MCU has internal Power-on reset (POR) and POR as well as Brownout reset (BOR) supply monitor with four configurable threshold voltages.
This reference design can be powered either by applying 5V through the USB Type-C connector or the marked headers or 3.3V at the designated header pins. See Section 4.1.1.2 for more details on the proper jumper connections for powering the board.
The USB Type-C interface can be used to program and debug the MSPM0G3507. This interface is isolated and can be used to provide 5V from the USB power to the system. If the 5V option is selected, the isolation of the USB Type-C interface is not in effect.
This reference design also comes with two options of transmitting the metrology parameters data over Bluetooth using either the CC2340 Bluetooth® low energy subsystem with all passives (discrete implementation) or a CC2340-based Bluetooth module.
The MSPM0+ MCU has internal Power-on reset (POR) and POR as well as Brownout reset (BOR) supply monitor with four configurable threshold voltages.
This reference design can be powered either by applying 5V through the USB Type-C connector or the marked headers or 3.3V at the designated header pins. See Section 4.1.1.2 for more details on the proper jumper connections for powering the board.
The USB Type-C interface can be used to program and debug the MSPM0G3507. This interface is isolated and can be used to provide 5V from the USB power to the system. If the 5V option is selected, the isolation of the USB Type-C interface is not in effect.
This reference design also comes with two options of transmitting the metrology parameters data over Bluetooth using either the CC2340 Bluetooth low energy subsystem with all passives (discrete implementation) or a CC2340-based Bluetooth module.