SLVUE37 October 2026
Figure 2-3 shows that the analog front end for current inputs is different from the analog front end for the voltage inputs.
This design has a 300µΩ shunt populated on the board for each phase and neutral. If desired the shunt can be replaced with another by desoldering the populated shunt and connecting the positive and negative leads from the new SHUNT sensor to the solder points.
Figure 2-3 Analog Front End for Current InputThe analog front end for current consists of footprints for electromagnetic interference filter beads (R74, R76, and R104), and an RC low-pass filter (R75, R77, C59, C60, and C61) that functions as an anti-aliasing filter.
Equation 2 shows how to calculate the range of differential voltages fed to the current ADC channel for a given maximum current.
Using the populated SHUNT value of 300μΩ, the input signal to the current ADC has a voltage swing of ±42.43mV when the maximum current rating of the meter, for example 100A, is applied. This relatively low voltage, when using GAIN = 16 is well within the required Full Scale Range of ±75mV, see the Full-Scale Range table in the AMC131M03 3-Channel, 64-kSPS, Simultaneous-Sampling, 24-Bit, Reinforced Isolated Delta-Sigma ADC With Integrated DC/DC Converter datasheet.
| GAIN SETTING | FSR |
|---|---|
| 1 | ±1.2V |
| 2 | ±600mV |
| 4 | ±300mV |
| 8 | ±150mV |
| 16 | ±75mV |
| 32 | ±37.5mV |
| 64 | ±18.75mV |
| 128 | ±9.375mV |