SNAA420A June 2025 – August 2025 HDC3020 , HDC3020-Q1 , HDC3021 , HDC3021-Q1 , HDC3022 , HDC3022-Q1 , HDC3120 , HDC3120-Q1
For this water leak detection experiment, a few assumptions were made to narrow the scope of the testing:
A vent was incorporated in the enclosure for pressure equalization. This prevents pressure buildup as internal temperature changes. In the experiment, TI used a waterproof vent to allow dampened air exchange with the atmosphere, allowing for pressure equalization while blocking liquid water. While this constitutes a semi-open system, this assumption still allows the experimental results to apply to closed systems. Nominally sealed systems do not develop internal pressure. Even a closed system that was hermetically sealed at atmospheric pressure, when punctured during a leak event, does not see a pressure change occur.