SNLA473 November 2024 DP83867CS , DP83867E , DP83867IS , DP83869HM , DP83TC811S-Q1 , DP83TC812S-Q1 , DP83TC813S-Q1 , DP83TC814S-Q1 , DP83TC817S-Q1 , DP83TC818S-Q1 , DP83TG720S-Q1 , DP83TG721S-Q1
To measure the SGMII output of the PHY, use an oscilloscope to measure near the input pins.
The input to the TX_M and TX_P pins on the PHY needs to follow the minimum requirements shown in Figure 1-13.
Section 1.6.1 is a sample eye measured against the input requirement, with the y-axis measured in millivolts and the x-axis measured in ns. Since the mask fits in this eye, the mask meets SGMII input requirements.
Figure 1-14 SGMII Example Simulation If the PHY SGMII input does not meet the requirements shown above, there can be some issues with the layout. See Section 1.7 for more details. The PHY SGMII output can also be adjusted with the VOD swing registers.
For example, these settings can be changed by toggling bits 13 and 14 of register 0x428 in the DP83TG720S-Q1.
| Bits 14-13 | Register Value | SGMII Output Swing | Unit |
|---|---|---|---|
| 00b | 0x0002 | 1000 | mV |
| 01b | 0x2002 | 1260 | mV |
| 10b | 0x4002 | 900 | mV |
| 11b | 0x6002 | 720 | mV |