SNOS749G September 1995 – November 2025 LMC6772 , LMC6772-Q1
PRODUCTION DATA
If the input signal is very noisy, the comparator output might trip several times as the input signal repeatedly passes through the threshold. This problem can be addressed by making use of hysteresis as shown below.
Figure 6-3 Canceling the Effect of Input CapacitanceThe capacitor added across the feedback resistor increases the switching speed and provides more short term hysteresis. This can result in greater noise immunity for the circuit.