SNOSAV4C April 2008 – August 2026 LM7332
PRODUCTION DATA
The LM7332 can be used as a drive amplifier for SAR ADCs as shown in Figure 7-1.
The values of Rflt and Cflt depend on the ADC specifications, as well as amplifier gain bandwidth product (GBWP) and output resistance (RO). A single ground-referenced supply voltage is also common, allowing sampling of signals up to half that voltage with low distortion.
To determine whether or not the LM7332 is a practical driver for this application, one must compare the settling time of the amplifier to the acquisition time of the ADC with Equation 1:
where
Using a value of 12 bits for N and 1µs for tAQ, the GBWPmin must be greater than 5.7MHz. The LM7332 has a GBWP of 24MHz so LM7332 is indeed a practical driver for this application.
Next, determine the value of Cflt with Equation 2:
where
Using a value of 80pF for CSH, the value of Cflt must be between 1600pF and 4800pF. The LM7332 can drive a capacitive load of 2000pF with 5VPP and settle within 1µs, therefore select 1800pF as the nearest common capacitor value within the range.
Next determine the value of Rflt with Equation 3:
where
Using a value of 1800pF for Cflt, 5.7MHz for GBWPmin, and a value of 1Ω for RO the value of Rflt is determined to be 630Ω. Use closest value of 626Ω for a filter frequency (fflt) of 141kHz given Equation 4:
The last requirement is to drive input signals of 2.5VPP on a single 5V supply with THD+N less than –80dB.
Figure 7-2 shows the THD+N response of the LM7332 with a dual supply voltage of 16V. The LM7332 can maintain THD+N levels as low as –110dB for output levels up to 4VPP. Therefore, the final requirement has been met, and the LM7332 is a practical drive amplifier for the 12-bit SAR ADC in this design example.