SNVSCS6A March 2026 – August 2026 TPS7H1301-SP , TPS7H1302-SP
PRODMIX
The stability of the LDO is influenced primarily by the dominant load pole and zero for the output capacitor (PCOUT, ZCOUT) and the internal compensation network (PCOMP_INT, ZCOMP_INT). Figure 10-2 illustrates where the pole and zero of the output capacitor and the internal compensation pole and zero of the LDO are located.
The pole and zero of the output capacitor are calculated using Equation 22 and Equation 23:
Applying Equation 22 and Equation 23 results in the following location of the respective pole and zero:
The internal compensation network pole and zero are calculated using Equation 26 and Equation 27:
COTA is the error amplifier's output capacitance; which is specified by design to be 20pf.
Applying Equation 26 and Equation 27 results in the following location of the respective pole and zero:
When applying an external compensation network utilizing the STAB pin utilize Equation 30 and Equation 31: