SNVSCU1A July 2025 – November 2025 TPSM65610 , TPSM65620 , TPSM65630
PRODUCTION DATA
This example uses the adjustable output voltage mode. An external voltage divider must be connected between the output node and the FB pin, while Equation 5 and Equation 6 are used to determine the divider values.
Note that Equation 6 states that the parallel combination of RFBB and RFBT must be greater than 4kΩ and less than 100kΩ. This limit is required because the regulator must reliably detect the sate of the FB pin during the start-up sequence to set the output voltage mode correctly.
Because adjustable output voltage mode is chosen for this example, the values of RFBT = 205kΩ and RFBB = 39kΩ satisfy both Equation 5 and Equation 6.
See also Section 7.3.1.