SNVSCU9B May 2025 – April 2026 TPS7H4012-SEP , TPS7H4012-SP , TPS7H4013-SEP , TPS7H4013-SP
PRODMIX
The device generates an internal nominal 1.2V bandgap reference voltage, VBG. This is the voltage present on the REFCAP pin during steady state operation. A 470nF capacitor to ground is required at the REFCAP pin for proper electrical operation as well as to ensure robust SET performance of the device. This bandgap voltage is used to derive the nominal 0.6V reference voltage for the error amplifier, VREF(internal).
The reference voltage that is fed into the error amplifier is utilized to set the output voltage. However, error amplifiers have intrinsic offset, VIO, which contribute to the overall accuracy error. Therefore, the voltage that is actually used to set the output voltage is VREF(internal) + VIO. This combined value is defined as VREF and is designed to be the accurate value to set the output voltage. VREF is specified across line, temperature, and TID in the Electrical Characteristics. Because VREF is measured in an open loop configuration, the effects of switching frequency and load on VREF are not included in the specification. See typical graphs Figure 7-31 and Figure 7-32 which show the minimal affect of current and switching frequency on the output sense voltage. See Section 10.2.2.8 for more details on calculating the output voltage accuracy.