SNVSD08 February 2026 LM34938-Q1
ADVANCE INFORMATION
A sequential write operation is an extension of the single write protocol and shown in Sequential WRITE Starting at a Defined Register Address . If the controller does not send a stop condition after the device has issued an ACK, the device auto increments the register address by one and the controller is able to write to the next register.