SNVSD08A February 2026 – October 2026 LM34938-Q1
PRODUCTION DATA
For stable current loop operation and to avoid subharmonic oscillations, the slope resistor must be selected based on Equation 41.
For the calculation of the mSC value for the slope compensation, use the effective inductance at the maximum inductor current (set by the current limit). With a RCS of 4mΩ the current limit is set to 12.5A (typically). The inductance of the used inductor decreases to Leff =2.5μH at this peak current.
The next higher value has to be selected which is 0.5 and then be set through the I2C interface.