Figure 2-9 shows the reset architecture of the AM261x controlSOM.
The AM261x SoC has the following
resets:
- PORz is the Power-On-Reset for
the MAIN Domain.
- WARMRESETn is the Warm Reset to
MAIN Domain.
The PORz
signal is driven by a 3-input AND gate that generates a power on reset for the MAIN
domain when:
- The PMIC drives the NRES, MCU
Reset output signal low.
- The 1.25V buck regulator
outputs a low signal for the power good signal.
- The user push button (SW2) is
pressed.
The PORz signal is tied to:
- AM261x SoC PORz input
- OSPI Flash Reset
- BOOTMODE buffer output
enable
- SOM HD Connector J1
The WARMRESETn signal creates a warm
reset to the MAIN domain when:
- The user push button (SW4) is
pressed.
The WARMRESETn signal is tied to:
- AM261x SoC WARMRESETN output
- RESETz signal created from push
button + PMOS logic
- IO Expander reset
The AM261x controlSOM also has an
external interrupt to the SoC, INTn, that occurs when:
- The user push button (SW3) is
pressed.