SPAU024A April 2025 – January 2026
The AM261x controlSOM does not have an onboard LIN transceiver. To interface with the AM261x LIN peripheral, the AM261x controlSOM must be connected to the HSEC180ADAPEVM-AM2 and plugged into the TMDSHSECDOCK-AM263. The TMDSHSECDOCK-AM263 has an onboard 2-channel LIN transceiver.
One instance of LIN is that LIN1 is routed to the SOM HD Connectors for interfacing using the HSEC180ADAPEVM-AM2 and TMDSHSECDOCK-AM263 or a compatible baseboard. The LIN1 peripheral can be accessed through one channel of the 2-channel LIN transceiver on the TMDSHSECDOCK-AM263.