SPRAD66B February 2023 – December 2024 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
The region of the PCB used for LPDDR4 circuitry must be isolated from other signals. The LPDDR4 keepout region is defined for this purpose and example is shown in Figure 2-5. The size of this region varies with the placement and DDR routing. Non-LPDDR4 signals must not be routed on the DDR signal layers within the LPDDR4 keepout region. Non-LPDDR4 signals can be routed in this region only if the signals are routed on other layers separated from the DDR signal layers by a ground layer. No breaks are allowed in the reference ground layers in this region. In addition, a solid VDDS_DDR power plane must exist across the entire keepout region.